AXIS#.SAFEPARAM.SLS_#.FSOE

Description

Indicates if the Safely Limited Speed (SLS) function can be activated through FSoE. This parameter can only set to “Used” when FSoE is activated (SAFEPARAM.SAFEFIELDBUS.ACTIVATION is set to 1 – “Activated”).

Value Description

0

Not used

1

Used

 

Parameters Editor with the FSoE options shown and circled

Context

For complete SLS information refer to SLS (Safely Limited Speed).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLS_1.FSOE

315ch

03h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_2.FSOE

315dh

03h

Unsigned8

-

-

Read/Write

No

AXIS1.SAFEPARAM.SLS_3.FSOE

315eh

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_1.FSOE

325ch

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_2.FSOE

325dh

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLS_3.FSOE

325eh

03h

Unsigned8

-

-

Read/Write

No